• AD3552R does not "wake up".

    Hi,

    it is not possible to get the AD3552R running in my setup. I use QSPI, communication works proper (I'm able to set / reset registers, perform a RESET, see the /ALERT pin response etc.)

    Unfortunetly, the DAC provides no output signals, even the VCMn…

  • AD3552R: FAQ

     Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question.

  • AD3552R / AD3542R initialization sequence

    What registers need to be configured to get the AD3542R / AD3542R up and running?

  • AD3552R - sequencing for writing configuration registers

    Hi, 

    We are having difficulties when implementing AD3552R component.
    Is there a particular sequencing for writing configuration registers? Can an external feedback resistor be used?Thanks, Marlene.
  • AD3552R Simulation Model Advantages

    Diverging from traditional LTspice models for DACs, focusing on the product’s output stage with simulations covering performance such as headroom, footroom or settling times, the LTspice model for the AD3552R revamps these models with a more digital simulation…

  • AD3552R DAC Eval Board + SPH-H1. ACE Software Transaction Error

    Hello,

    We are evaluating the AD3552R DAC using the EVAL-AD3552RFMC1Z and SPD-H1.

    I downloaded and installed the latest ACE software (1.24.3098.1398) and connected the boards.

    ACE software is able to recognize the connected devices and I can fully navigate…

  • AD3552R DAC Eval Board + SPH-H1. ACE Software unable to set offset.

    Hello,

    We are evaluating the AD3552R DAC using the EVAL-AD3552RFMC1Z and SPD-H1.

    I downloaded and installed the latest ACE software (1.25.3217.1403) and connected the boards.


    The 1kHz 'DefaultSingleTone' vector is added and 'Play' is clicked and we can…

  • DAC performance graphs

    Are there performance graphs or plots available for the AD3552R DAC at frequencies greater than 100KHz?  Looking for performance from 100KHz to 5MHz.

  • Precision Wide Bandwidth Measurement and Drive

    There is an ever-increasing desire for more insights and more data from the world around us. To extract those insights, it can mean that instruments must carry out both time domain and frequency domain analysis. The underlying circuity in the instruments…

  • DAC Output not updating

    I am able to read and write single-byte registers but the output is not updated when I write a word to the DAC register.

    The AD3552R is configured in address decrementing mode by default. When addressing a multi-byte register, the address of the MSB…