• AD2S1205

    (datasheet,英文版)

  • AD2S1205

    Dear Sir/Madam,

    I use FPGA drive ad2s1205   for testing fault detection delay time . When EXC , SIN, COS ar NC,  the fault detection
  • RE: AD2S1205: incremental encoder emulation failure

    Hi,

    The AD2S1200 and the AD2S1205 should produce very similar encoder outputs.

    As regards compatibility between the two devices the AD2S1205 input range is wider than the AD2S1200 and covers the range of the AD2S1200 so that should not be an issue.…

  • RE: AD2S1205, without using excitation for resolver ?

    The synthetic reference improves performance and accuracy by reducing the phase shift between the excitation and the sine, cosine inputs.

    If you are not using the excitation from the AD2S1205 you need to synchronize the AD2S1205 excitation to the source…

  • RE: What are the differences between the AD2S1200 and AD2S1205 ?

    Both devices offer very similar performance level however the AD2S1205 converter was released to automotive through AECQ-100. The AD2S1205 IC is newer device which has some advantages over older AD2S1200 like:

    1. The AD2S1205 has an extended input signal…

  • Reference buffer

    Is necessarily to use reference buffer with the AD2S1205/AD2S1210 converter ?

  • Is it necessary to use 68 kOhm resistors with the AD2S1205?

    Is it necessary to use 68 kOhm resistors with the AD2S1205?

  • RE: AD2S1200,AD2S1205,AD2S1210芯片选型

    AD2s1205可以直接替换AD2s1200,相比AD2s1200,AD2s1205最大跟踪速度更高,增加汽车认证级版本

    AD2s1210是最新的解码芯片,相比AD2s1205,支持最高16bit分辨率模式,精确度更高,用户自定义故障阈值寄存器,灵活性更高

  • Synchro/Resolver-to-Digital Converters

    Can we use AD2S1205 to synchronize two old DC motors suffering from field weakening effect?

  • RE: AD2S1205 startup issue

    Jackson,

    I apologize but I misinterpreted your original message, I had incorrectly assumed the EXC/EXCN pins were loaded by the resolver but I missed that CLKIN was not toggling..   As the clock is not starting up (CLKIN) you can expect that EXC, EXCN…