• RE: A2B TEST USING ADZS-AD2428MINI‎

    Thank You Very Much Ken. One More Questions Do I Need To Use Sigma Studio? And Somewhere Has Sample Codes With Table To Initialize AD2428W?

  • Hi ADI members,

    In the AD2428W evaluation board, there are lots of inductors and capacitances, please refer to the following picture, can you explain the function of these inductor and capacitance?

    thanks.

  • A2B ADV2428W- Data band width 50Mbps - for High speed GPIO transmission

    Hi , 

    We would like to send I2S-MCLK 49MHz from A2B-Master node to A2B-Salve node thought Pin13 (DTX1/IO4). 

    Could AD2428W send high speed MCLK through GPIO pin?

  • RE: [ADAU1761] It can't sound from HP out

    Hello,

    I've tested with my A2B master board and slave board.

    EVAL-AD2428WD1BZ is my master and EVAL-AD2428WB1BZ is my slave.

    Actually, I asked, what is your master board.

    But it's okay. I will share my code to your e-mail.

    In the EVAL-AD2428WB1BZ…

  • RE: The difference between AD2428WCCSZ & AD2428WCCSZ01

    Hi Henry.

    As indicated in the selection guide you referred to, the xx suffix affixed to Automotive product numbers is the silicon revision, so the AD2428WCCSZ01 is for silicon revision 0.1. If there is no suffix (AD2428WCCSZ), it is revision 0.0. The…

  • A2B hotpluggable or how to resync the bus?

    Hello,

    we just started today with A2B Bus using master and slave eval boards equipped with AD2428W devices.

    We just made some tests with audio streaming from salve to master, thereby we saw that the bus won't resync after unplugging and re-plugging of…

  • A2B ALSA DRIVER FOR ARMV7A 32BIT PROCESSOR

    Hello

    Here We Are Designning A Car Stereo Using A2B AD2428W And Looking For ALSA Driver Support ARM 32 Bit Processor. I See Some Similar Requirement Has Submit By Previous Posts In Community But So Far I Don't See Any Definite Usable Official Resources…

  • SigmaStudio and A2B Software for Windows 7 (32-bit)

    Hello everybody

    I'm going to start working with A2B AD2428W IC but we need to do it on a Windows 7 32-bit operating system, processor: Intel(R) Core(TM) i7-4770S CPU @ 3.10 GHz 3.10 GHz. Unfortunately I can not update the Operating System at this moment…

  • AD2433W using TX1/RX1 TDM interface

    Hello,

    I am using the AD2433W as a master. I wish to use the RX1/TX1 TDM interface of the A2B module instead of RX0/TX0. I am using TDM16 mode. I have a single A2B slave - AD2428W

    For the RX part, I do not receive any downstream data at my slave A2B device…