• RE: ADSZ-SC589 MINI boot problem without A2B node connected

    I resolved the issue. If the initialisation of the A2B node fails, the following function will return an "EVENT FATAL";

    // Initiate A2B bus configuration sequence
    			if ((ad2425_result = ad2425w_load_init_sequence(&ad2425w,
    															…

  • A2B Class-D Amplifier Module for the SHARC Audio Module now available

    The A2B Class-D Amplifier Module is an expansion board for the SHARC Audio Module (ADZS-SC589-MINI) that leverages ADI’s low-latency audio A2B bus technology. It features an AD2425W A2B transceiver (serving as an A2B slave) and accepts audio over…

  • A2B: AD2428W and EVAL-AD2425WBZ Linux driver code

    We use AD2428W as master and EVAL-AD2425WBZ as slave, cound you please provide Linux driver source code of this?

    BRs

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…
  • RE: 360°全方位的ADI汽车电子技术是怎样炼成滴?围观抢百元京东卡

    (1)BMS系统。

    ADI 有完整的 BMS 系统(双精密 ADC 和精密基准电压源、ARM 处理器、闪存和收发器)集成到一个市场主导型系统级封装 (SiP) 中,树立了 12V 停止-启动 BMS 的行业标准。主要芯片有AD7284,ADUC7039等。

    (2)磁力轴位置传感器。

    ADI 的 AMR 磁力轴位置传感器提供实现这些目标所需的精度、快速响应能力和稳固性。主要芯片有AD2S1205,ADA4571等。

    (3)电流检测放大器。

    ADI 的电流检测放大器具有出色的性能,适用于各种汽车和电源管理应用…