FAQ
Question:
Can all the NC (No Connect) lines pin5 to pin8 be tied together to a floating plane of copper? by MHermoso
____________________________________________________________________________________________
Answer:
The AD22100’s NC pins are not internally…
Hi.
I plan to use AD22100S temperature sensor in my application. I have some questions about it.
1. Could I use this sensor in case of high vibration (about 15g, 2-2000 Hz)? Datasheet just don't contains info about vibration immunity.
2. Could…
The AD22100’s NC pins are not internally connected to the die. So, they can be left floating or tied to any potential like VDD or GND. To ensure that the sensor accurately measures the temperature of the PCB/heatsink, the device GND pin should be connect…
Hi, Carmen.
Apologies for missing this. Peak reflow is listed as 260C when you check for package information here, so the JEDEC standard J-STD-020 would be a good reference.
Are you planning to do measurements where the IC will be immersed? The datasheet…
ADXL78 |
ADXL001 |
ADXL278 |
ADIS16223 |
ADIS16240 |
ADIS16209 |
ADIS16203 |
ADIS16201 |
ADXL193 |
ADISEVAL |
ADXL1005 |
ADIS16000 |
ADIS16210 |
ADIS16227 |
ADIS16228 |
ADIS16229 |
ADIS16305 |
ADXL1001 |
ADXL1002 |
ADXL1004 |
ADXL103 |
ADXL151 |
A… |