• Ad202 isolation amplifier

    I've seen several sites about price and not clear about how many channels have the AD202. They change according to models?


  • AD202 isolation amplifier

    hello

    i want to know more about transformers used in ad202 please...specially the material used as the transformer's core...

    thanks for your help

  • AD202 power supply current requirements

    I'm looking to properly size my power supply. I am hoping to run 12 AD202KNs off of a single power supply. I see in the data sheets the AD-246 requirements but I wasn't clear on whether they applied to AD202s from a +15 V source.


    How much…

  • AD202的输出问题

        电路原理图如图1所示。输入输出曲线如图2所示,AD202输入为电源信号,当其接入500ms瞬时负载时,输入信号会出现电压拉偏,而输出信号则出现更大的信号幅值拉偏,不再是11的传输关系。图3为检测5脚电压曲线,图4为检测6脚电压曲线,均在同一时刻出现幅值拉偏。

    图1

    图2

    图3

    图4

  • ¿Cuantos canales de entrada tiene el AD202?

    ¿Cuantos canales de entrada tiene el AD202?

  • AD202: potting material, Cleaning possible - Pins internally connected

    1).  Is the part suitable to be processed through a co-solvent cleaning process
    after the devise is fitted/solder to a board in order to remove any flux
    residues from the soldered connections?


    2). The device seems to be potted…
  • AD202JY: Input overvoltage protection

    Using unity gain as your data sheet RevB page 5 Figure 5. Vin in the range 0 to
    +5v, have attenuated battery voltage with a potentiometer. Concerned for
    overvoltage protection, is there any protection built into the Ad202 ? Have
    tried…
  • RE: 请大家推荐一款模拟输入,经过隔离后模拟输出的ADI芯片

    隔离的话,有两个方案。一个是在模拟信号这边就隔离,要选择模拟隔离放大器,像AD202,AD215这样的器件。

    还有一个方案是在数字侧进行隔离,上述ADuM的型号都可以使用。

    另外,我们也有隔离ADC,像AD7403,输出的是数字码流,需要做抽取后得到真正的数字输出。

  • 0-20mA to isolated 0-5V

    Do you have an One Chip solution to Transform an 0-20mA Signal to an isolated
    0-5V Signal (or something similar)? So it's a Sensor we want to read out with a
    voltage Module for further use. The Isolation is very important because we have…
  • ADAS3022转换结果回读

    项目背景,电动汽车充电桩的检测装置,主要用来测试充电桩反馈信号的电压信号,以及充电电压及电流值。(交流电信号通过AD202与后级隔离)

    硬件设计描述:

    AGND,DGND,COM,AUX-,NC接地

    VDDH:+14.5V

    VSSH,TPAD:-14.6V

    AVDD,DVDD:5.0V

    VIO:3.3V

    REFIN:+2.512V

    测得:

    RCAP,DCAP,ACAP:+2.5xxV

    REF1,REF2:4.09xV

    接口跟FPGA之间采用ADuM241E隔离。

    软件…