• AD1953 with Blackfin 561 , No audio data in one channel

    I am working on a Project in which 2 channel audio is streamed from Blackfin 561 to AD1953 using SPORT0 and SPORT1. I can able to hear the audio output via left channel (VoutL+/-) but nothing heard in the Right channel (VoutR+/-) Let me know your suggestions…

  • RE: AD1953 intreface with BF 561

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: interfacing blackfin with ad1953 sigma audio processor

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD1953 & USBi

    Is USBi communication supported with the AD1953 dsp chip in SigmaStudio 3.6? The application won't allow me to connect the two in the hardware communication.

  • No audio data on the output of processor AD1953

    Hello,

    I'm working on a project of a digital equalizer with processor AD1953. I designed my own hardware and tried to resuscitate the equipment, but there is no audio data on the outputs of AD1953, just a DC component. To be more specific a voltage 0…

  • RE: ADAU1761 can run SRS WOW HD ?

    The list of algorithms available for each processor is changing with each build (as we port some algorithms to new cores, or develop completely new algorithms), so it would be difficult to keep an up-to-date list.

    However, here's a recent list of some…

  • How many instructions can be executed per sample in SigmaDSP?

    Calculating IPS (Instructions Per Sample)

    The number of instructions that can be executed per sample depends on three things:

    • The core frequency of the SigmaDSP you are using (as you have it configured in your system)
    • The size of the program memory of…
  • TAGS LIST: Processors & DSP

    ADUC812
    ADUC814
    ADUC816
    ADUC824
    ADUC831
    ADUC832
    ADUC834
    ADUC836
    ADUC841
    ADUC842
    ADUC843
    ADUC845
    ADUC847
    ADUC848
    ADUC7019
    ADUC7020
    ADUC7021
    ADUC7022
    ADUC7023
    ADUC7024
    ADUC7025
    ADUC7026
    ADUC7027
    ADUC…
  • RE: I get the following error message when I link-compile-download. "System.componentmodel.win32exception (0x80004005): The system cannot find the file specified at system.diagnostics.process.startwithcreaterprocess(processstartinfostartinfo) at syst...

    Dave,

    Attached is a dspproj file.

    I have these same issues with any of my current dsp project files.

    I am running: win10 64 bit, SigmaStudio 4.1, HP Zbook workstation. Ethernet connection to HW (Simon-Kaloi rPod) audio playback and show control unit…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…