• AD1854: SPI port unused

    At this moment I’m working at a prototyping-project in which I use a DA
    converter of Analog Devices. The DAC in question is the AD1854KRS.
    I’ve downloaded the datasheet from your website. In my project I have no
    interest in controlling…

  • AD1854 to AD1852

    Hi

    My customers chose the AD 1854 as an alternative to the AD 1852, which became an EOL.
    The customer buffered the audio output of the AD 1854 and the customer gave control signals and data to the AD 1854 in the same way as the AD 1852.
    However, AD 1854…

  • 2008-06-10 05:29:18     Audio noise AD1854

    2008-06-10 05:29:18     Audio noise AD1854

    Zaahir Khan (INDIA)

    Message: 56919   

    Hello All,

    I am using BF561 ezkit, customised board.

    Having AD1854 audio chip.

    When we are running mp3 song. It sounds OK to us.

    But when we are running 1k mp3 sine tone…

  • 2009-03-17 14:51:57     use AD1854 with AD1836

    2009-03-17 14:51:57     use AD1854 with AD1836

    damien OLLIVE (UNITED STATES)

    Message: 71136   

    hi,

    i need your advise to tell me if i am on the write way to do what i want and if yes how to solve my problem.

    i am on a custom board witch is close to the…

  • 2011-10-15 19:02:24     ad1854 sound 2010-Rc5 bf537

    2011-10-15 19:02:24     ad1854 sound 2010-Rc5 bf537

    Chris Page (UNITED STATES)

    Message: 103879   

    I am currently updating our current kernel to 2010-RC5. The sound drivers have completely changed. We have succesfully ported the ad1836.c file previously…

  • 2006-06-20 10:53:14     AD1854 Audio Out on BF537 EZLITE

    2006-06-20 10:53:14     AD1854 Audio Out on BF537 EZLITE

    Falk Hatzfeld (GERMANY)

    Message: 9182    Compared to the 537 STAMP the 537 EZLITE has an audio DAC (and ADC) polulated. Is it possible to use this AD1854 with uClinux as well? (Driver / settings)?

  • RE: BF-537 EZKIT driver for AD1854 or how to use AD194x driver

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • 2008-06-10 12:46:48     On BF537 EZ-KIT, AD1854 and uClinux

    2008-06-10 12:46:48     On BF537 EZ-KIT, AD1854 and uClinux

    Nicola Bonelli (ITALY)

    Message: 56941   

    In some previous posts I have read that it's possible to use the built in AD1854 DAC on BF537 EZ-KIT

    running uClinux.

    In particular it should be…

  • 2011-10-20 00:20:25     codec alsa 2010 rc5

    2011-10-20 00:20:25     codec alsa 2010 rc5

    Chris Page (UNITED STATES)

    Message: 104003   

    I am starting new thread regarding codec ad1854 and alsa for uClinux version 2010R1-RC5. I am porting the ad1836 codec to work with ad1854. I have converted it to…