• Does the AD1852 accept SPDIF format?

    Does the AD1852 accept SPDIF format?

     

    Yes the AD1852 does accept SPDIF format (refer to Figure 29 on page 16 of
    datasheet RevA)

  • AD1852: ESD sensitivity, HBM model data missing from datasheet

    I couldn't find in datasheet the parameter called Human Body Model which
    informs me about ESD sensitivity of IC. In data sheets for most other
    components, HBM parameter appears in Absolute Maximum Ratings list. Could you
    let me know what is…

  • Trimming or Minimizing the DC Offset of AD1852

    I am measuring about -53mV at both the channel of outputs of the opamp for OUTPUT BUFFERS AND LP FILTER of the AD1852 DAC.

    this value is about typical value given in the datasheet.


    Is there a method to trim or minimise this DC offset for AD1852?


    I have…

  • AD1854 to AD1852

    Hi

    My customers chose the AD 1854 as an alternative to the AD 1852, which became an EOL.
    The customer buffered the audio output of the AD 1854 and the customer gave control signals and data to the AD 1854 in the same way as the AD 1852.
    However, AD 1854…

  • RE: About AD1852 pin#6

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD1852 is showing NRND on your website , please advise reason for NRND also please advise replacement for AD1852JRSZRL

    AD1852 is showing NRND on your website , please advise reason for NRND also please advise replacement for AD1852JRSZRL

  • Noise in the begin signal DAC AD1852

    Hello! I use DAC AD1852. I transmit data - 128 zero and then sine. But when I change pin RESET I see noise on output (about 1.44 ms) and then I see my signal. I don't understand why always noise become in the begin signal. I try using pin MUTE in the…

  • Noise in the begin signal DAC AD1852

    Hello! I use DAC AD1852. I transmit data - 128 zero and then sine. But when I change pin RESET I see noise on output (about 1.44 ms) and then I see my signal. I don't understand why always noise become in the begin signal. I try using pin MUTE in the…

  • AD1852 3.3V I2C

    Hello guys,

    So I have the following situation:

    - I am using a Bluetooth module that output I2C justified data (48kHz sampling rate and a variable bit rate {between 16-24-32 bits} depends on played format) to the AD1852. The I2C lines are pulled high…