• AD1583: Solder temperature

    What is the peaksolder reflow temperature can be used for AD1583. If thermoprofiles standard J-std-200 for AD1583. Information that is given in the documentation (page 8) AD1583  I can't understand. There given: Lead Temperature, Soldering, Vapor Phase…

  • AD1583: Temperature coefficient out of the specified values

    Ten samples were tested in following configuration:
    +5V regulated supply decoupled with 100uF
    output loaded with 1.5kOhm and 1uF
    As clearly seen from the attached charts something really bad happens with the
    part when temperature falls…
  • RE: Replacement Part for MAX6035-3

    Hi Roberto,

    I moved this question to keep the two issues separate for other customer who may be searching with similar questions.

    The AD1583 looks to be a close replacement at first glance, so please look at this and see it this solves your questions…

  • [征文] IN118的基准源用AD的芯片,上面写着D6B,困饶我很久了 AD5312


    这个芯片(AD9833)的名字我猜的,可忽略看,如果是这个芯片,左看右看也不知是干吗呢?

  • ADI芯片辨识、型号查找

    看看截图:

  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…