• RE: what is the input signal frequency range in AD10242 - 12 Bit 40M Samples per Second Analog to Digital Converter (ADC) Evaluation Board

    search on analog.com

    Selection Table for Standard High Speed A/D Converters >20 MSPS | Parametric Search | Analog Devices

  • Power Consumption in AD10242

    Hello!

    As per datasheet:

    AD10242 : 12 BIT, 40MSPS, Dual ADC, 1750mW Power

    If I use this ADC at a lower sampling rate say 10 - 20MSPS (if its possible) and single channel,  then power is reduced or not? If yes, then let me know.

    Thanks,

    Regards,

    Dars…

  • RE: An issue about AD10242

    Hello,

    The AD10242 has a logic compatibility for only TTL/CMOS. The Logic Low level must be between 0 - 0.8 Volts and the logic High must be between 2.0 to 5.0 Volts.

    John

  • AD10242时钟差分输入的问题

    在使用AD10242时遇到问题。

    在时钟输入上你们提供了单端输入的电平标准,即当cmos电平0.8-2v,这个在手册中已经说明,但是并未提及差分时候的标准。但是在手册的Figure 11 中显示可以使用标准ECL GATE 驱动时钟,但是一般认为ecl的摆幅只有0.8v

         我的问题是:1 ecl差分接入的0.8v摆幅是否可以驱动ad10242,lvpecl电平是否可以满足标准?

                               2 figure 11 中的终端电阻510欧姆是怎么计算出来的

                                      谢谢

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…