• AD10200 application issue

    Dear Sir/Madam,

    I wonder how to configure the PIN1 of AD10200.

    Thanks.

  • Queries about AD10200

    Dear Supporter,

    I used AD10200 in my project. I tested AD10200 with signal generator. The sampling clock is 105MHz. FFT N=65536.

    When I input 10MHz sine wave, the FFT result looks good. Please see below pic.

    but when I input 41MHz, 71MHz or 105MHz…

  • AD10200 input range problem

    The AD10200 input rated range in the datasheet is 2.048V, in the example from -1.024 to +1.024V, but I don't know if it can support 0-2.048V analog input, or even 0-2.5V analog input.

  • AD10200输入量程问题

    datasheet中AD10200输入额定量程为2.048V,举例中从-1.024到+1.024V,但是我不知道是否能够支持0-2.048V的模拟输入,甚至于0-2.5V的模拟输入。

  • AD10200应用电路问题

    1. AD10200管脚1的该如何接?

    2. AD10200数据手册中应用电路里的引脚与器件引脚图不匹配,如何区别?

  • AD10200: Are the two channels fully independent?

    There are two channels in AD10200. I only want to use one channel. I found out
    that there are two AVCC pins and two DVCC pins. I wonder if he can only power
    up the AVCC and DVCC pin of the channel I use while grounding the other channel
  • 关于AD10200的一个问题

    请问AD10200芯片的采样时钟输入是否可以是差分正弦波,而不是差分方波信号?

    这两种波形,那种的ENOB参数更好一些?能相差多少?

  • 关于AD10200空余脚的处理

    以下问题:

    1)AD10200管脚1的作用是什么,在实际的电路使用中,应该如何处理?

    2)模拟信号输入端是否为CMOS电路,A路、B路其中一路输入悬空时,悬空管脚如何正确的处理?

    3)采样时钟输入端是否为CMOS电路,A路、B路其中一路输入悬空时,悬空管脚如何正确的处理?

    另外,一般CMOS电路输入管脚悬空时,应该如何正确处理?具体原因是什么?能否详细解释?

    谢谢!!!!

  • AD10200: Channel-to-Channel isolation test with AINA2 and AINB2

    On the evaluation board are two SMA connector on the pin 6 (AinA1) and pin
    62(AinB1). They are also shown at the schematic on page 12 of datasheet (Rev A).

    These two pins AinA1 and AinB2 are "Not Connected" on the Pin Configuration …
  • 关于AD10200开盖内部发现有腐蚀性元素硫

    5962-9961003HXA(AD10200TZ/QMLH)一批货里面开盖后内部发现有腐蚀性元素硫,另外一批货没有腐蚀性元素硫。

    请相关技术人员帮忙解答以下问题:

    1.这个货AD 原厂出厂是本身含有腐蚀性元素硫的么?

    2.内部含有腐蚀性元素硫会不会影响货的使用性能?

    3.为什么有些货含有硫,有些没有含有硫?

    4.产品是有升级换代么?所以才会出现有些含硫有些不含硫?

    5.关于此产品,AD出厂前有相关测试报告么?