• RE: Dual AD9361 Vivado Build Error

    Hi Rajeesh,

    Got the same problem as jlavie.

    Have changed the reference design and some of the file names with respect to my design changes.

    Got DRC errors as said in the above post, so tried like this:

    set_property -dict [list CONFIG.PCORE_0_IODELAY_GROUP…

  • RE: ADXL362 Z data incorrect

    Hi STallur,

    I put the ADXL362 board on the desk, and make the board horizontally as possible as I can.(It's hard to make perfect flat).

    The voltage is 3.3V for above test result.

    Today, I got new sample(#549) from avnet. and I replace the #547…

  • ad9361 - linux- LPF digital filter unexpected response

    Hello,

    I designed a low pass filter for ad9361(fmcomms3) with Matlab Filter wizard. I join below the generated ftr file (fs= 13.5MHz, Start 1.5M, Stop 2M).

    I'm interested only on Rx side and I check the output result on FPGA (Xilinx Zynq) through ILA…

  • RE: Microcontroller to ADSP 21469 ez-kit lite via I2C

    Hello,

    As there is no default programmable interrupt priority for TWI, you may need to assign it to any of the programmable interrupt. In the below code I have assigned TWI interrupt (selection code is 0x17) to programmable interrupt 0 (PICR0 [4:0]),…

  • RE: I2C Interrupt on EZ board 21486 not firing

    Hello,

     

    As there is no default programmable interrupt priority for TWI, you may need to assign it to any of the programmable interrupt. In the below code I have assigned TWI interrupt (selection code is 0x17) to programmable interrupt 0 (PICR0 [4:0]…

  • Dual AD9361 Vivado Build : Critical Warning

    Hi Guyz,

    Got the same problem as:


    Dual AD9361 Vivado Build Error


    Have changed the reference design and some of the file names with respect to my design changes.


    In the above said link,  axi_ad9361_0 has been used as variable.

    Referring that…

  • RE: Questions about LTM4622A

    Hi SYoung,

    thank you very much and sorry for the delay. Finally I had time to install LTSpice and try it. It looks impressive, but there are a few questions:

    1. Specific capacitors were used for the simulations. Can I change them? Does the program really…

  • GPIO interrupt

    Hello!

    I have a basic question about the GPIO interface. I'm using a ADRV9361 SOM with the ADRV1CRR breakout board and I'd like to use one of the DIP switches (SW0) in my C application. The gpio file in /sys/kernel/debug already lists SW0 at gpio…

  • RE: Accessing SYNC_IN on ZedBoard and FMCOMMS4

    The ZYNQ GPIO controller has two sets of pins, the MIO pins and the EMIO pins. The MIO GPIOs are directly connected to fixed output pins of the package, while the EMIO pins are connected to the FPGA fabric and can be routed to any FPGA pin.

    root@analog…
  • RE: Errors compiling facedetect with bfin-uclinux-g++

    Thanks for your answer.

    This means that I should reconfigure opencv, but when I do configure like this:

    ./configure --host=bfin-linux-uclibc --without-gtk --without-carbon --without-quicktime --without-1394libs --without-ffmpeg --without-python --without…