[#5924] Scheduling error shows up sometimes in latest trunk
Submitted By: Vivi Li
Open Date
2010-02-22 23:14:17
Priority:
Low Assignee:
Barry Song
Status:
Open Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Category:
N/A Board…
We have had generally good luck with the background measurement feature in the 7623. We are using the sdk repeater implementation. We have run across a couple of behaviors that warrant questions:
2009-05-07 03:30:00 Regarding USB detection from my application
Hari Prasad (INDIA)
Message: 73791
Hi,
I have to develop an application that is to work with USB contents. When a USB device is connected to my BF527 device, I have the following…
[#6527] Some error message shows up when scan usb storage devices with isp1760
2011-04-06 06:11:05 Close Date
2011-06-15 02:19:44
Medium Assignee:
Bob Liu
Closed Fixed In Release:
Found…
[#4579] Blackfin camera driver fails in current trunk
Submitted By: Mike Frysinger
2008-10-30 11:25:53 Close Date
2008-11-01 02:43:22
Michael Hennerich
Found In Release…
Are you really sure that you use the proper device tree?
I rebuild everything - and attached my boot log for your reference.
Linux version 4.6.0-10610-g0c79cd7 (michael@mhenneri-D04) (gcc version 4.9.2 (Sourcery CodeBench Lite 2015.05-17) ) #2882 SMP…
We do not use a filter file - we use the driver from ADI. Do we need a specific filter file?
The AGC works OK for high level of input signal, down to -80dBm then it start deteriorating the CINR down to -100dBm
I am sending you the registers map in…
I skip a calibration step and after this function - "ad9361_tx_quad_calib(phy, real_rx_bandwidth, real_tx_bandwidth, -1);" power consumer of 1.3V is about 0.001A.
I attach part of schematic for TX_VCO_LDO_OUT, for RX is same.
The register dump…
虽然这是一篇针对AD7780在电子秤系统中的辐射抗扰度分析的经验文章,里面经验之谈,同样适合其他电子产品设计中的辐射抗扰度参考。好文推荐之!
AD7780是一款包含PGA的低噪声、低功耗、24位∑-△型转换器。AD7780用于低端到中端的电子秤系统。作为发布过程的一部分,测试了电子秤系统的辐射抗扰度。本应用笔记介绍如何实现AD7780的最佳抗辐射性能,在设计印刷电路板(PCB)的过程中考虑了电路板布局和元件放置的影响。根据IEC 61000-4-3标准对整套系统(ADC、PCB和称重传感器…
Hello Aaron,
I get the following log when I try to compile gSoap for Blackfin. To make the configuration I used the following command "./configure --host=bfin-linux-uclibc --build=x86_64-pc-linux-gnu --prefix=/usr --sysconfdir=/etc --datadir=/usr/share…