• LOg amplifier AD 606

    Gentlemen,

    as a Radio Amateur I am doing some developmentin controlling output signalof radio equipment.I made a circuit by using AD´s log amp AD 606. Recently I checked the flatness of Vlog versa frequency between 2 to 30 MHz.Here I realized a variation…

  • RE: BF-606 Interrupts

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: BF-606 shared memory

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • [#5350] Build bf526 kernel failed at traps.c

    [#5350] Build bf526 kernel failed at traps.c

    Submitted By: Vivi Li

    Open Date

    2009-07-13 23:33:13     Close Date

    2009-07-13 23:36:09

    Priority:

    Medium High     Assignee:

    Nobody

    Status:

    Closed     Fixed In Release:

    N/A

    Found In Release:

    N/A     Release:

    Category:

    Make …

  • [#5342] branch head kernel build fails at traps.c on bf526 ezbrd

    [#5342] branch head kernel build fails at traps.c on bf526 ezbrd

    Submitted By: Mingquan Pan

    Open Date

    2009-07-12 23:52:07     Close Date

    2009-07-13 22:47:42

    Priority:

    Medium High     Assignee:

    Robin Getz

    Status:

    Closed     Fixed In Release:

    N/A

    Found In Release:

  • RE: AD9361 Filter Wizard does not format FIR filter coefficients as int16

    Hello,

    Thanks a lot for your reply.

    After trying the code on the new branch, we can confirm that the FIR filter coefficients are now inside the correct int16 range.

    Nevertheless, we have noticed a decrease in the gain of the filter of about 10dB compared…

  • Algorithm Details in Noise Removal block

    Hi,

    Just a very quick question.

    The "Algorithm Details" section of Noise Removal block in this page of WiKi

    https://wiki.analog.com/resources/tools-software/sigmastudio/toolbox/adialgorithms/noisereduction

    It says,

    Algorithm Details

    Toolbox…
  • RE: ADSP SC 573 SPI DMA mode

    Hi Nikhil,

    Could you please provide the below details to us. This would be helpful for us to assist you further

    1. SPI buffer size for your application

    2. SPI configuration snippets for both source and destination modules.

    3. Is there any specific reason…

  • RE: AD9164 stuck at CGS

    AD9164 ACEPlugin can record the startup sequence and generate the sequence. below is from ACEPlugin. it seems like you programmed 0x230 with the wrong value. it should be 0x28. 

    W 0 18
    W 200 1
    R 6
    W D2 52
    W D2 D2
    W 606 2
    W 607 0
    W 604 1
    W 58 3
    W 90 1E…

  • RE: ad9361 filter design wizard

    Hi Travis,

    I have the same question, but as you said the minimum sampling rate is 520.3333kHz, I designed the filter with data clock as 520841.

    I saved the coefficients as .c files and copied the generated AD9361_TXFIRConfig and AD9361_RXFIRConfig structure…