• AD9129 Evaluation Board & Xilinx ML-605 Reference Design Questions

    Hi,

    I'm using AD9129 Evaluation Board, DAC-FMC Interposer & Xilinx ML-605 Reference Design

    and I have several questions.

    I followed the step-by-step procedure outlined on your wiki (http://wiki.analog.com/resources/fpga/xilinx/interposer/a…

  • AD9129 Evaluation Board & Xilinx ML-605 Reference Design Questions

    Hello Analog Devices

                I’m a physics undergraduate at California Polytechnic and am currently working on the AD9129 Evaluation Board to Xilinx project (https://wiki.analog.com/resources/fpga/xilinx/interposer/ad9129). We have all the listed components…

  • AD9129-EBZ, ML-605 Reference design, Loading user samples to SDRAM

    Hello

    My customer has the AD9129-EBZ board connected to the ML-605 via the DAC FMC Interposer board.

    He is using the ADI Reference Design for the ML-605, which is available on http://wiki.analog.com/resources/fpga/xilinx/interposer/ad9129

    On the Wiki…

  • AD9122 EVALUATION BOARD, DAC-FMC INTERPOSER & XILINX ML-605 REFERENCE DESIGN

    Hi,

    I've downloaded that reference design but it lucks of sw code - it has only XPS design. Where can I find the software for Microblaze for that design?

    Best regards,

    Dominik

  • Miss ISE project files when I downloaded reference design tar file of AD9467 Native FMC Card / Xilinx ML-605 Reference Design

    Hi,

    Why can I find the whole package as you indicated?

    Thanks.

    Kev.

    Tar file contents

    The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool…

  • Can I use KC705 replace ML605 in the refrence design of AD9129 Evaluation Board?

    Hey :

            I have read the refrence design of ad9129 evluation board as follow:

    AD9129 Evaluation Board, DAC-FMC Interposer & Xilinx ML-605 Reference Design [Analog Devices Wiki]

    in the design it use ml-605,but I have no ML-605 in my hand, I want to…

  • RE: ADV7184 video switching problem

    i don't cut off any camera's power supply; after switching, the value of 0X10 register remain at 0X4D always;

    but 0X13 register changes from 0X6D  to 0XED 、0X8D 0X8D、0XAD.ultimately remains at 0XED;

    the following message comes from console ;the…

  • RE: AD9129 not working

    The AD9129 DACCLK input can receive signals as low as -10 dBm with only a couple of dB loss in phase noise performance. Are you following the Quick Start Guide procedure for power up and configuration of the eval board, or do you have a different sequence…

  • RE: Error -22 writing to channel "sampling_frequency" value may not be supported.

    fir.txt
    RX 3 GAIN -12 DEC 4
    TX 3 GAIN -12 INT 4
    RRX 800000000 25000000 8333333 4166666 2083333 520833
    RTX 800000000 25000000 8333333 4166666 2083333 520833
    BWRX 433256
    BWTX 433256
    114,114
    -98,-98
    157,157
    -154,-154
    -23,-23
    -330,-330
    -346,-346…

  • RE: Using no OS driver with custom h/w in verilog

    Thank you for reminding me Vivado does not support ML 605. However I am in plan to get Zynq board.