• RMS Current Control Based on LTC1968

    Dear Team,

     

    I want to make current control via MOSFET based on LTC1968. The load will be full wave rectified sinusoidal ( not filtered ) and frequency will be max 400hz.

    My design is in the attachement.

    1. I have used U1-LTC1968 and U2-LT1782 for RMS to…
  • RE: LTC4020 | 1. 48V/10A Input, 13S Li-Ion Battery, 54.6V Vout |2. 24V/10A Input, 10S Li-Ion battery, 41.6V Vout


     PDF PDF

    Please find the attached schematic. I have uploaded two file SCHEMATIC1 (Input48V/10A | Output: Vout:54.6V/3A, Vbatt: 54.4V/2A) and SCHEMATIC2 ( Input24V/10A | Output: Vout:41.665V/3A, Vbatt: 41.48V/2A). 

     

  • External dimensions of EVAL-ADV7625

    Hi,

    I have a question about ADV7625.

    I would like to know the external dimensions of the evaluation board EVAL-ADV7625.

    https://www.analog.com/media/en/technical-documentation/user-guides/EVAL-ADV7625-SMZ_UG-603.pdf#page=8

    Best Regards,
    Naohisa

  • RE: ADRV9002 Linux Kernel Driver for Arria 10 SoC

    I grep'd through my kernel source and I have exactly the same instances as in your master branch kernel.

    $ grep -nr adrv9002_axi_hdl_loopback
    drivers/iio/adc/navassa/adrv9002_conv.c:603:void adrv9002_axi_hdl_loopback(struct adrv9002_rf_phy *phy,…

  • Error when trying to load profile from iio-osc. Linux Ubuntu 18 matlab R2020a HDL 2019_r2

    Below is my profile

    and image from std. out of iio-osc from host machine.

    I added .ini suffix to the profile and still no luck. Before doing so iio-osc said it couldn't find the file.

    <profile Talise version=1 name=Tx_BW200_IR245p76_Rx_BW50_OR61p44_ORx_BW200_OR245p76…

  • RE: LMR applications using the ARV9002 -- Receive adjacent channel and spurious rejection test data available (per TIA standards)?

    Hi Eric,

    1. The limits specified in TIA standards are tested with analog audio SINAD and tone test pattern BER, it involves the performance of baseband demodulating and signal processing which should be implemented in FPGA(outside the ADRV9002 scope)…

  • RE: ADuCM355 Cyclic Voltammetry Example Current Conversion Formula

    Hello,

    I am running the following example: C:\Analog Devices\ADuCM355V2.2.0.39\examples\M355_CycloVoltammetry

    According to this post: https://ez.analog.com/analog-microcontrollers/precision-microcontrollers/f/q-a/164963/calculatoin-of-current-through-lptia…

  • RE: Clarifications regarding ADP 5091 eval board usage

    Hey kevin,

    I tried the number you earlier provided.  +862123208066,

    Altough, both the numbers i could not find in whatsapp.

    Can you please ping me to my whatsapp at +91-988 603 1118.

    On Wed, May 23, 2018 at 2:11 PM Kevin.Yao <

  • Comment on 05-17 Wearable and Clinical Vital Signs Monitoring.pdf

    Hello Ever.q21,

    I’m including the subject matter expert and webcast presenter, Jan-Hein Broeders, to this email.

    Please ask Jan-Hein your question and he will be happy to answer it.

    Thanks!

    Patrick

    Patrick Kusior

    Webcast & Video Manager

  • RE: AD9371 Device Clock Selection Issues

    I've attached the 84, 134.4, and 168 device clock profiles all with a RX IQ rate of 42MSPS. These are all selectable device clocks from the AD9371 profile wizard.

    For the 84 MHz profile, the Linux kernel function xilinx_xcvr_calc_cpll_config() located…