• 2009-10-28 14:44:44     ADV7180 driver availability

    2009-10-28 14:44:44     ADV7180 driver availability

    Randy Young (UNITED STATES)

    Message: 81821   

    I am working on a project that will likely use the ADV7180 video decoder.  I see that there is a driver in the source tree for the ADV7183B, but I could not…

  • 2010-06-09 04:44:44     Populating /dev with mdev

    2010-06-09 04:44:44     Populating /dev with mdev

    Vitaly Izbash (RUSSIAN FEDERATION)

    Message: 90218   

    Hi, friends...

    I can see a SATA drive in /sys/block directory (sda, sda1, sda2).

    Then I try to populate it into /dev with a command mdev -s.

    As a…

  • RE: ADV7842/44 Deinterlacing

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • 2008-08-07 06:03:44     data transfer

    2008-08-07 06:03:44     data transfer

    Pranay Upadhyay (INDIA)

    Message: 60094   

    Hello sir,

        I have compiled the u-boot 2008R1, and formed the uboot binary file .After loading the u-boot, I am trying to sending the file but  data is not transmitting through…

  • 2008-06-21 07:54:44     u-boot size

    2008-06-21 07:54:44     u-boot size

    Appalayagari Sreedhar (INDIA)

    Message: 57674   

    Hi,

    How much space u-boot occupy default?. In my custom board i have 64MB sdram and flash is connected in BMODe:00.

    after booting i could see the u-boot loaded at the…

  • RE: ADV7181C Cap pins(38/39/44)

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • 2009-04-24 09:44:53     signals

    2009-04-24 09:44:53     signals

    vijai ragavan (INDIA)

    Message: 73159   

    hai,

    I have some doubt regarding messages on uclinux.

    I am using the following code for message create ,pend and post .

    Message create:

    #define MESSAGE_Q

    signed int messageid…

  • 2009-12-09 11:19:44     pthread_cond_timedwait

    2009-12-09 11:19:44     pthread_cond_timedwait

    Filip Vanalme (BELGIUM)

    Message: 83305   

    Hi,

    I'm still using 2006R1. Is it possible that there's a problem with the function pthread_cond_timedwait in that version ?

    I notice that, sometimes, all…

  • 2008-06-10 03:45:44     poll_wait

    2008-06-10 03:45:44     poll_wait

    Pranay Upadhyay (INDIA)

    Message: 56894   

    Hello  sir,

        For reading and writing the frame continuously from the ppi driver.May I used the poll_wait function.If we can use then in which function I use this function. As I…