• Do you have a receiver for ARINC 429 busses with the DO-160 lighting protection?

    Do you have a receiver for ARINC 429 busses with the DO-160 lighting protection?

  • [#4111] MUSB fails to build for BF524/BF526

    [#4111] MUSB fails to build for BF524/BF526

    Submitted By: Mike Frysinger

    Open Date

    2008-05-17 09:49:09     Close Date

    2008-05-22 06:08:53

    Priority:

    Medium     Assignee:

    Bryan Wu

    Status:

    Closed     Fixed In Release:

    N/A

    Found In Release:

    N/A     Release…

  • RE: ADIsimpll仿真

    ADISimPLL没有集成AD9957. 要仿真AD9957内部的PLL性能可以用类似的PLL芯片,如AD9525+external VCO. Kv 选择在429~850MHz/ (参考手册Table 1)。

  • RE: Can't load profile.txt to ad9371 profile.config

    6646.profile.txt
    <profile AD9371 version=0 name=Rx 100, IQrate 122.880>
     <clocks>
      <deviceClock_kHz=122880>
      <clkPllVcoFreq_kHz=9830400>
      <clkPllVcoDiv=2>
      <clkPllHsDiv=4>
     </clocks>
    
     <rx>
      <adcDiv=1>
      <rxFirDecimation=2>
      <rxDec5Decimation…

  • CN-0429 - setvbias limits

    Hello,

    I have the boards from the Circuit Note 429 and I am trying to set the voltage bias on one of the boards to -600mV.

    When using the command: "setvbias -600", the response is "Sensor bias set to -600 mV". However, using the "ReadConfigs…

  • RE: EVAL - AD5933EBZ Rev C

    Hello, I downloaded the program link in the upper, and when I open it in the program tells me "Firmware failed to download-Check USB connections", this is due to?

    I canceled this error, commenting, and the program gives me another error "Form1…

  • Profile loading error ad9371

    I have created my profile using  MATLAB Profile/Filter Generator for AD9371 . When i load the profile as shown below 

    Loading a Profile

    This specifies any shell prompt running on the target

    root@analog:/sys/bus/iio/devices/iio:device3# cat…
  • RE: ZC706 with AD9371

    Yes we are matching TX and RX. i ha

    rx_tx_6144.txt
    <profile AD9371 version=0 name=Rx 50, IQrate 61.440>
     <clocks>
      <deviceClock_kHz=76800>
      <clkPllVcoFreq_kHz=9830400>
      <clkPllVcoDiv=2>
      <clkPllHsDiv=4>
     </clocks>
    
     <rx>
      <adcDiv=1>
      …

  • RF发送器 脉冲信号


    项目设计需要一个用于胎压监测系统的RF发送器,发出信号频率为429±3MHZ,发送周期为20us,脉冲信号宽度为1us.请问采用什么型号的发送器,和射频开关配合可以实现上述要求?或除了发送器配合射频开关方法外,还有没有别的更优越的方法?

  • RE: error in writing in order "WritetToControlRegister" with EVAL-AD5933

    Hello, I downloaded the program link original, and when I open it in the program tells me "Firmware failed to download-Check USB connections", this is due to?

    I canceled this error, commenting, and the program gives me another error "Form1…