• What's the difference between the ADuM1440/41/42 and the ADuM1445/46/47?

    What’s the difference between the ADuM1440/41/42 and the ADuM1445/46/47?

     

    All devices in the family contain a refresh circuit to guarantee dc correctness
    at power up. If no pulses are received on the secondary side of the transformer
    for…

  • ADuM144x Low Power Digital Isolators:  What's the Difference between ADuM1440/41/42 and ADuM1445/46/47?

    All devices in the family contain a refresh circuit to guarantee dc correctness at power up. If no pulses are received on the secondary side of the transformer for approximately 200 µs, the input side is assumed to be unpowered or nonfunctional…

  • adc coverter with c 42 part marking

    hi

    i have a single channel 10pin MSOP  ADC converter with part marking C 42 but i cant find exact part number to buy it again.

    can anyone help me about this?

    thanks 

  • ADV7511 fails to read register 42

    We've a custom box with several ADV7511 chips outputting video from an FPGA.

    We initialize the ADV to run at a constant resolution DVI output 1024x768p60, and this works okay.

    To detect the hot-plug status, we poll register 0x42 every few seconds…

  • RE: 2008-01-02 14:07:42      JACK on Blackfin?

    This question has been closed by the EZ team and is assumed answered.
  • (ADV7281AM)Can we delete "42 00 10 ; INSEL =unconnected input [INSEL Switch]"?

    Hi !

    I have a question.

    Our customer are using ADV7281AM with full differential CVBS for automotive.

    They are using this script.

    **********************************************************************************

    ##07_CVBS DIFFERENTIAL FAST SWITCH ##

  • 2010-03-26 09:42:36     gdbserver

    2010-03-26 09:42:36     gdbserver

    Filip Vanalme (BELGIUM)

    Message: 87737   

    We have a multi-threaded application. I would like to debug it with gdb. Therefore, I start gdbserver on our board and use Eclipse's debugging environment. I can set a breakpoint…

  • 2011-01-24 15:42:52      http:// docs.blackfin.uclinux.org/

    2011-01-24 15:42:52       docs.blackfin.uclinux.org/

    Blair Fredericks (CANADA)

    Message: 97652   

    Hi,

      docs.blackfin.uclinux.org/

    This site appears to be down?

    Does any one know what is going on with it?

    Blair

    QuoteReplyEditDelete

    2011-01-24 15:45:…

  • 2008-05-20 09:42:18     link error

    2008-05-20 09:42:18     link error

    Slava Zhuiko (RUSSIAN FEDERATION)

    Message: 56053    hi! After adding the next portion of code to my current project I got the following error message: undefined reference to `___sync_fetch_and_add_4'. Thanks in advance…

  • 2009-11-01 17:03:42     GMP linking

    2009-11-01 17:03:42     GMP linking

    Sergio Decherchi (ITALY)

    Message: 81981   

    Hello,

    I am new at uClinux and I am trying to cross-compile and link the following simple program (prova.c):

    #include <stdio.h>

    #include <gmp.h>

    int main()