• 2010-02-09 02:41:41     BFin527 Board Reset directly issue.

    2010-02-09 02:41:41     BFin527 Board Reset directly issue.

    Xin Xin (CHINA)

    Message: 85786   

    Hi,

        We do bt download, the Bfin527 devel-board resets directly. No system crash message, just reset to uboot, and booting.

    We check the power is ok, and test…

  • Vdropout data of ADP1740/41

    Hi

    I'm DFAE in Japan. I'd like to propose the small solution size LDO to our customer competing with TOREX XC6230.

    https://www.torexsemi.com/file/xc6230/XC6230.pdf

    I'd like to know the drop out voltage ADP1740/41 at the condition as follows.…

  • ADE 7758: 41 bit energy register

    AWATTHR, BWATTHR, CWATTHR registers represent the upper 16 bits of the 41 bit energy register, as given on pg 32 of the datasheet (http://www.analog.com/static/imported-files/data_sheets/ADE7758.pdf). But then how will the value in 16-bit registers be…

  • NDS&PSRR data of ADP1740/41

    Hello,

    I only found the NSD & PSRR data about ADP1740/1741 in datasheet as shown below.

    Could you please provide NSD & PSRR graph data of ADP1740/1741 for the following conditions?

      - V_dropout = 0.3V, V_out = 2.5V and 3.3V

    Thanks in advance…

  • 2009-07-29 09:56:41     PG11

    2009-07-29 09:56:41     PG11

    Steven Sheppard (UNITED STATES)

    Message: 78166   

    Using the BF537_STAMP board:

    Under the simple-gpio driver, which gpio# would be pg11?  Is there a table of these somewhere?

    QuoteReplyEditDelete

    2009-07-29 10:08:25     PG11

  • 2011-04-20 07:02:41     coeff_iirdf1_fr16

    2011-04-20 07:02:41     coeff_iirdf1_fr16

    Marcin Salata (POLAND)

    Message: 100040   

    Hello

    I want to use coeff_iirdf1_fr16 but when I try compile my program I've got this error:

    /opt/uClinux/bfin-uclinux/bfin-uclinux/runtime/usr/lib/libbfdsp.a(coeff_iirdf1_fr16…

  • 2008-07-17 06:41:24     sureshkumar

    2008-07-17 06:41:24     sureshkumar

    suresh kumar (INDIA)

    Message: 59012   

    I installed the eclipse into my host linux pc.

    If ,I try to configure the eclipse for debug.i can't do that.

    In the Project name field enter the name of your program.

    Un…

  • 2010-01-21 04:41:15     thttpd

    2010-01-21 04:41:15     thttpd

    Parimala Baggiri (INDIA)

    Message: 84934   

    Hello,

                Why is thttpd is not updated to the latest version(thttpd-2.25b)? With the existing version when I run thttpd apllication I get the following error

    root:/> thttpd

  • 2010-09-02 04:41:56     menuconfig

    2010-09-02 04:41:56     menuconfig

    Filip Vanalme (BELGIUM)

    Message: 93066   

    I have a problem when executing make menuconfig :

    In the first stage, I select [*] Customize Application/Library Settings

    Then I get this error message :

    FVA@tlv-thc-lx-01…

  • 2010-05-05 05:31:41     hylafax + iaxmodem

    2010-05-05 05:31:41     hylafax + iaxmodem

    Alec Joseph Rivera (PHILIPPINES)

    Message: 89150   

    Hi all:

    *sorry for cross-posting*

    I've recently been able to make the recent iaxmodem version on baps. On my test, I was able to get asterisk to dial it too…