• RE: ADV7181C SVGA issues

    Hi Guenter,

    With regard to the PWRDWN signal, I can control this from my ADM1064 power sequencer device. Will test this next week.

    We wait 10ms after an I2C reset before writing additional commands to the device.

    I could not publish the schematics…

  • RE: CSC for SD encoder adv8005

    sure,

    this is the configuration:

    i2c16w 1a e828 10
    i2c16w 1a 1a04 22
    i2c16w 1a 1a05 00
    i2c16w 1a 1a06 04
    i2c16w 1a 1a07 6c
    i2c16w 1a 1b48 08
    i2c16w 1a 1b30 87
    i2c16w 1a 1b31 06
    i2c16w 1a 1b32 19
    i2c16w 1a 1b33 9e
    i2c16w 1a 1b34 1f
    i2c16w 1a 1b35 5d
    i2c16w…
  • ADV8005 Eval SD encoder line fliker

    hi,

    I am using the eval ADV8005 to convert from 1024x768P60 to 576i.

    I am using the following configuration:

    i2c16w 1a e828 10
    i2c16w 1a 1a04 22
    i2c16w 1a 1a05 00
    i2c16w 1a 1a06 04
    i2c16w 1a 1a07 6c
    i2c16w 1a 1a39 0a
    i2c16w 1a 1a3b b7
    i2c16w 1a 1a3c …
  • Eval ADV8005 Analog Output scaling problem

    Hi,

    I am scaling a 1024x768@60p DVI video input to an analog 576@50i output (with EVAL ADV8005-8N).

    command used:

    -src HDMI 1

    -mainvsp 576i50

    -out comp 1 main

    The conversion has the following two problems:

    1) is present a bar on top of video that is…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • RE: ADV8005 test pattern

    I did some addictional test. Since I am able to obtain a valid output through a demoboard, I dumped the content of its registers, and they are attacched below. I'm in the process of rewriting (and veryfing) the same values on the processor I'm using in…