• Is there supposed to be a statement: Link.Talise.GetAgcPowerRegisters(Power_AGC) on page 146 UG-1295 at the beginning of the section: Program data structure to powerclass

    Is there supposed to be a statement: Link.Talise.GetAgcPowerRegisters(Power_AGC) on page 146 UG-1295 at the beginning of the section: Program data structure to powerclass? 

    At the beginning of the section: Program data structure to AGC Control class (UG…

  • RE: EVAL-HMC774ALC3B

    Hi, 

    The 2.92mm is SRI CONNECTOR 25-146-1000-92 and SMA is CINCH 142-0701-851.

  • [#4585] warning with GPIO code for BF51x in current trunk

    [#4585] warning with GPIO code for BF51x in current trunk

    Submitted By: Mike Frysinger

    Open Date

    2008-11-01 02:44:16     Close Date

    2008-11-03 05:13:07

    Priority:

    Medium     Assignee:

    Bryan Wu

    Status:

    Closed     Fixed In Release:

    N/A

    Found In Release:

    N/A     Release…

  • Advantiv EDID Editor (EEditGold) wrong unit in text report

    , found a tiny bug in the text report files:

    Descriptor Block #4
      Monitor Range Limit - 0xFD  
      Default GTF  
        Range Limit  
          Min V rate=20 kHz  
          Max V rate=146 kHz  
          Min H rate=15 kHz  
          Min H rate=160 kHz  
          Max Clock =600 MHz 

          Min V rate and Max V rate…

  • VisualDSP License File

    The license file is not valid. 

    We have provided the validated license.dat file for the license serial number ADI-146-256-222233604-3452 with the host ID . Please find the attached validated license.dat file.
    Can you please replace the existing one with…

  • RE: How can I get BOM for HMC8205BF10 EVAL PCB?

    Hi Zormax,

                         the circuit board is 10 mils thick. Not really able to mill a slot. From a manufacturing stand point the jumpers were the most cost effective option. The BOM is attached.

    Regads,

    Jim B

     PDF

  • RE: AD9783 Noise Spectrum

    Hello ,

    Apologies for the delayed response.

    Kindly see attached file which includes Phase noise data with Fout at 10MHz output and clock at 150MHz, 250Mhz & 350MHz. Unfortunately I was not able to get data at 500MHz because of the limitation of my…

  • AGC Parameters using Python Script

    Trying to enter AGC Peak/Power mode (with Gain table and external attenuator) with Python Script.  Using the Python script on pages 146-149 of the ADRV9009/8 Hardware Reference Manual (UG-1295), I am getting an index System.IndexOutOfRangeException after…

  • RE: HMC1087 Eval Board Connector

    Hi sweentj_96,

    The SRI P/N is: 25-146-1000-92

    Thanks,

    DanO

  • ADF4360 Phase Noise Spec

    Hi, I am currently using the ADF4360-9 to generate an LO ref in the range 146-152 MHz. My phase noise requirements are quite strict so have ended up running the VCO at double this and using the Divout f/2 output to get a slight improvement in noise performance…