Post Go back to editing

EVAL-SDP-CH1Z data streaming

Category: Software
Product Number: hw-sdps

Hi,

Can someone please advise if the SDP-H1 can be configured as described in the thread below to allow data streaming? 

Thank you!

(+) Streaming data with the AD4134 eval board and SDP-H1 - Q&A - Precision ADCs - EngineerZone

"Hello,

I'm evaluating the AD4134 as a candidate ADC for a low-noise measurement we are developing. I managed to get the combination of EVAL-AD4134 and the SDP-H1 evaluation boards working and talking to each other. However, I can only record a maximum of ~100ksamples with the ACE software that ships with the SDP-H1. What I'd like to do is to stream data off the EVAL-AD4134 / SDP-H1 and write it to disk for later processing, can I reconfigure the SDP-H1 to function in this way? I believe USB supports enough bandwidth for me to stream 4 channels of 24-bit data at ~1 MSPS so I don't expect that to be a bottleneck, but ideally, I'd like to use the on-board memory buffer on the SDP-H1 such that I do not suffer any discontinuities. Browsing the forum, I came across this thread but some of the links there are broken, so I figured I'd ask if anyone has had a similar application requirement and managed to get the combination of SDP-H1 and EVAL-AD4134 working.

Thanks!"