Post Go back to editing

EVAL-AD5781 can't be controlled by ACE

Category: Hardware
Product Number: AD5781

Hi,

I've got 1 EVAL-AD5781SDZ(REV B) and 1 EVAL-SDP-CB1Z.

And I power EVAL-AD5781SDZ through J11 with 5V supply.

I connect EVAL-AD5781SDZ J4 with EVAL-SDP-CB1Z J14.

I connect USB of EVAL-SDP-CB1Z with my laptop.

I opened ACE and it can detect EVAL-AD5781SDZ.

But I can't control AD5781 with ACE software, the screen is shown below.

The connection is as described in the user guide

EVAL-AD5781SDZ (Rev. 0) (analog.com)

And I measured, VDD=+13.7V, VSS=-14V, IOVCC=3.3V.

What could be wrong?

What else do I need to check?

Thread Notes

  • Hi,

    It seems you have followed the userguide default values.

    1.) Can you share the board view or what comes after you click EVAL-AD5781 plug in?

    2.) Have you checked if you are using the latest version of the plug in and ACE? you may do this by going "Home" -> "Plugin Manager" -> "Available Updates". To update ACE itself, click "Check Updated" on the lower left of the ACE UI.

    3.) Have you connected any voltage reference daughter board to the EVAL-AD5781SDZ, can you share the setup if so?

    Br,

    Den