Post Go back to editing

EVAL-SDP-CB1Z + dual EVAL-AD7616

Thread Summary

The user inquired about using a single EVAL-SDP-CB1Z to control two EVAL-AD7616 boards for acquiring data from 24 analog channels. The final answer indicated that the existing evaluation software cannot support this setup. The user then asked for alternative approaches, such as APIs or libraries to control the SDP-B.
AI Generated Content
Category: Hardware
Product Number: EVAL-AD7616, AD7616

Hey there,

I just started using the EVAL-AD7616 with the SDP-B controller (EVAL-SDP-CB1Z) on Windows PC. I need to convert 24 analog channels, so I'm planning to use 2x AD7616 to have up to 32 channels.

I would like to use a single master board (i.e., 1x SDP-B) to control at the same time 2x EVAL-AD7616 and acquire data via the evaluation software. First, can I do this? I understand that connectors A and B of the SDP-B share some pins, and there are 3 SPI interfaces. Can I connect 2x EVAL-AD7616 to the same SDP-B evaluation board? Can the software control the two of them?

Hope my questions are clear!

Best,

MPE

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.