Hi, I want to use EVAL-AD7606B-FMCZ which is compatible with SDP-H1.
I already have SDP-B and AD7606-4SDZ.
I'm wondering now that Eval-AD7606B-FMCZ is compatible with SDP-B.
AD7606-4
Production
The AD7606/AD7606-6/AD7606-4 are 16-bit, simultaneous sampling, analog-to-digital data acquisition systems (DAS) with eight, six, and four channels, respectively...
Datasheet
AD7606-4 on Analog.com
AD7606B
Recommended for New Designs
The AD7606B is a 16-bit, simultaneous sampling, analog-to-digital data acquisition system (DAS) with eight channels, each channel containing analog input...
Datasheet
AD7606B on Analog.com
Hi, I want to use EVAL-AD7606B-FMCZ which is compatible with SDP-H1.
I already have SDP-B and AD7606-4SDZ.
I'm wondering now that Eval-AD7606B-FMCZ is compatible with SDP-B.
Hi smLee.
I support the SDP-B and SDP-H1, but I am not familiar with the AD7606B or the AD7606-4. The connectors used on the Evaluation boards are completely different - EVAL-AD7606B-FMCZ uses an FMC-LPC connector and the AD7606-4 eval board uses the SDP-120 connector.
Even if you were to bypass the FMC connector, the SDP-H1 was most likely chosen for the extra throughput or improved timing available on the FPGA. The FPGA functionality is only available on the SDP-H1.
So, I do not expect that you can make the AD7606B work with the SDP-B.
There are alternatives to the SDP-H1 for the AD7606B. If you have already chosen a different FPGA board, then you may be able to implement your own custom solution using the No-OS drivers or the Linux drivers.
Hi smLee.
I support the SDP-B and SDP-H1, but I am not familiar with the AD7606B or the AD7606-4. The connectors used on the Evaluation boards are completely different - EVAL-AD7606B-FMCZ uses an FMC-LPC connector and the AD7606-4 eval board uses the SDP-120 connector.
Even if you were to bypass the FMC connector, the SDP-H1 was most likely chosen for the extra throughput or improved timing available on the FPGA. The FPGA functionality is only available on the SDP-H1.
So, I do not expect that you can make the AD7606B work with the SDP-B.
There are alternatives to the SDP-H1 for the AD7606B. If you have already chosen a different FPGA board, then you may be able to implement your own custom solution using the No-OS drivers or the Linux drivers.