Post Go back to editing

EVAL-SDP-CB1Z

Category: Software

I attached an EVAL-AD7616SDZ to the EVAL-SDP-CB1Z und I would like to transfer Data from the CB1Z over UART to another computer.
Is their a way to program the CB1Z so that I can get Data from CB1Z over UART to another computer?

What kind of IDE can i use for that?

Kind regards

Markus

Parents
  • Hi,

    Support for the SDP varies depending on what you are intending to do with the board. If you are using it as intended - together with one of the daughter cards, LabView, etc - support is handled through the EngineerZone, here:
    ez.analog.com/.../sdp

    This community is monitored and supported by SDP engineers and they will be able to answer any questions you have.

    If you are intending to use the Blackfin SDP as a standalone, low-cost, BF527 Evaluation platform together with the VisualDSP++/CCES tools, your correct support channel would be through Applications Support, or Processor Tools Support, under the same guidelines as any other Evaluation Board: if the question is tools related, send it to us(Processor.tools.support@analog.com). If the question is specific to the application you are developing it should go to Apps(Processor.support@analog.com).

    We have a couple of FAQs on the EngineerZone to help customers get started with the BF527 SDP-B, either with VisualDSP++ or open source tools, on the EngineerZone, here:
    FAQ: Using the Blackfin SDP-B as a BF527 Evaluation Platform:
    ez.analog.com/.../faq-using-the-blackfin-sdp-b-as-a-bf527-evaluation-platform

    Regards,
    Divya.P

  • Hallo,
    Can you provide any example code for piping out data on UART with the SDP-CB1Z?
    If there is something like that possible?

    Kind regards 

    Markus

Reply Children
No Data