Hi,
It seems my SPD-S board does not succeed to connect to the attached CN-0276 board.
The connection to the SPD-S from the PC seems OK. I believe so since the board shows up fine in the Windows device manager and when I disconnect the CN-0276 I get a message telling me that I need to connect a daughter board, so there is some intelligence on the SPD-S telling me via USB that the daugheter board is missing.
When I have the CN-0276 connected and start the CN-0276 evaluation software I get the message "Connect to the SPD Board Failed"
See bottom left in the picture below.
I have:
- Checked that the 120-pin connector is properly connected.
- Checked that I have the .NET 3.5 installed and enabled.
- Tried connecting another CN-0276 (I have two), but that did not help.
- Using both 12 V and 6 V input voltage (power) on the CN-0276, but that did not help either.
So - I'm a bit at a loss on what to do next. Buy a second SPD-S, hoping that the one I have is faulty?
Or - is this a "known problem"?