Post Go back to editing

problem with CN0399 SDP-S and SDP-Z

Category: Software
Product Number: CN0399 SDP-S AND SDP-Z

Dear reader,

 I can't get the combination of SDP-S (controller) and SDP-Z (RF unit) to work.

My PC has Windows 7

When I connect the SDP-S/SDP-Z to a USB port, the correct PC System messages come up:

Analog Devices System Demonstration platform SDP-S

 At Details it says:

Creation date 02-12-2020

Version 2.14.0.0

After starting GUI ADI_SDP_Writer1 ( version April 12, 2017,9.39.52) and pressing button “CONNECT”

comes after a few seconds: SDP connected.

After this, according to the procedure, some calibration value entered with the GUI.

 

If I now measure the power, a very wrong value appears on the GUI display.

As an example I take the measurement at 1 GHz with a known connected level of 0 dB

A positive number of +39.5 dB appears on the GUI, so 39.5 dB is too high.

 If you offer a level of -10 dB at the input, the GUI will indicate +29.5 dB, so 39.5 dB is too high.

At an input of -20 dB, the GUI indicates + 20.0 dB, so 40 dB is too high.

With no input signal, the GUI shows +5.0 dB?

 In the table 3PointCal-LUT, the frequency of 1 GHz has the following value:

1000.60.5-34.0330578512397.58.2,-35.3780068728522,,895,2059,2664.

 I think the last 3 values ​​represent the counts of the AD converter. And if this assumption is correct

then the combination SDP-S and SDP-Z would work well. But the GUI makes the calculation mistake.

 I can't figure out what and where it goes wrong can you help me?

I am an amateur (72 years) and have tried a lot but I can't get it to work properly.

 Thank you in advance for your response. Best regards,

 LLLRRR

 

 

 

Parents
  • Hi,

    It's not clear if the calibration file is being written correctly. Can you delete the contents of the file are start again?

    Regards,

    Kieran 

  • Thanks Kieran for your response.

     

    I have deleted and re-created the calibration file several times. The result remains wrong. The manual of the RF unit (SDP-Z) contains the fttp address where the software can be downloaded. This software would be suitable for Windows 7. This software package also contains a driver with an installation program. After installation, the driver has serial number 2.1.2.0 (date 24-10-2013).

     

    On the site below from analog.com

    www.analog.com/.../sdp-s.html

     

    is also a driver to load this can work with Windows 7 and higher . Its version number is 2.14.0.0 Creation date 02-12-2020.

     

    I have performed all experiments, including the re-creation of Calibration files, several times with both drivers on a Windows 7 PC. The result remains wrong.

     

    I don't know how to interpret the data in the Calibration files. It seems to me that the last 3 values ​​are the counts of the A/D converter and that is in line with the specifications. So the hardware seems to be working fine.

    Even if you lower the transmit level 10dB, the much too high false dB indication changes exactly 10dB.

     

    The button in the GUI for connect also works well. But something goes wrong with calculating the measured dB value.

     

    The GUI is an EX file and would have been written in MS visual studio. There is also a PDB file, a Manifest file and a vshost file. No source code is included. So find out for yourself where things are going wrong. It is also not possible to determine how the calculation of A/D counts to dB will go.

     

    Who oh who knows the solution

     

     

    Thank you very much with kind regards,

     

    lll.rrr

     

     

Reply
  • Thanks Kieran for your response.

     

    I have deleted and re-created the calibration file several times. The result remains wrong. The manual of the RF unit (SDP-Z) contains the fttp address where the software can be downloaded. This software would be suitable for Windows 7. This software package also contains a driver with an installation program. After installation, the driver has serial number 2.1.2.0 (date 24-10-2013).

     

    On the site below from analog.com

    www.analog.com/.../sdp-s.html

     

    is also a driver to load this can work with Windows 7 and higher . Its version number is 2.14.0.0 Creation date 02-12-2020.

     

    I have performed all experiments, including the re-creation of Calibration files, several times with both drivers on a Windows 7 PC. The result remains wrong.

     

    I don't know how to interpret the data in the Calibration files. It seems to me that the last 3 values ​​are the counts of the A/D converter and that is in line with the specifications. So the hardware seems to be working fine.

    Even if you lower the transmit level 10dB, the much too high false dB indication changes exactly 10dB.

     

    The button in the GUI for connect also works well. But something goes wrong with calculating the measured dB value.

     

    The GUI is an EX file and would have been written in MS visual studio. There is also a PDB file, a Manifest file and a vshost file. No source code is included. So find out for yourself where things are going wrong. It is also not possible to determine how the calculation of A/D counts to dB will go.

     

    Who oh who knows the solution

     

     

    Thank you very much with kind regards,

     

    lll.rrr

     

     

Children
No Data