Hi,
I wanted to externally power the AD4020 eval board. After going through the datasheet of the eval board I figured out that I had to do the following changes.
Switch SL9 for +Vs
Switch SL8 for -Vs
Switch SL7 for Vdd
Switch LK2 for Vref
On the eval board it looks like
+Vs = 7V
-Vs = -2.5V
Vdd = 1.8V
Vref = 5V
I provided the following voltages
+Vs = 5V
-Vs = -5V
Vdd = 1.8V
Vref = 5V
After doing these changes I connected it to the ADI-SDP board to test it. I gave a 40kHz sine wave as the input to the ADC. However this is the output I got
The output is varying between two codes (0 to -1) when the input is a sine wave of 200mV amplitude and 40kHz frequency. However the frequency of the output is correct. So I thought I blew up the ADC while doing the changes to the board. So I replaced the ADC and tested it again. The same problem persisted, only this time the output was a square of the right frequency but was varying between 0 and -500000 instead of 0 and -1.
Any idea why this is happening? What am I doing wrong? I also tested to see if the signal was actually reaching the ADC properly. And it is. So I am clueless as to what is wrong. Please help me debug this.
Regards,
Mohan Prabhakar
Edit Notes
Adding tags for internal tracking purposes[edited by: tschmitt at 3:53 PM (GMT 0) on 25 Feb 2020]