Post Go back to editing

ADAR1000 SPI

Thread Summary

The user is seeking example source code to control the ADAR1000 via SPI without using a GUI. The final answer indicates that the code was emailed to the user. Accompanying answers suggest using the provided SPI programming example in the datasheet and adapting a GPIO control function for the ADAR1000, with the CSB pin needing to be controlled correctly. Additional users have requested copies of the code, and one user has shared a GitHub repository with their implementation.
AI Generated Content

 Hello, I am using ADAR1000 but unfortunately, there is no reference source code. I could not find anywhere. Just we have SPI PROGRAMMING EXAMPLE in the Datasheet. I want to make and control the SPI communication protocol without using GUI. Can you provide example source code?

Best Regards.

Parents Reply Children