Post Go back to editing

ADRV9009 profile wizard crashing - recent behavior

Category: Software
Product Number: ADRV9009
Software Version: 2.4

the profile configuration wizard seems to have recently started crashing (closing) when I input the above config parameters and click generate profile (with default parameters it works).  I tried reinstalling matlab runtime R2014b and doing a system restore to a version prior to some recent windows updates but its still crashing.   thanks for any suggestions

Thread Notes

Parents
  • Same problem here! I came here to try and find out what to do because I'm baffled. 

    Talise Configuration Wizard version 2.4 installed. 

    It has worked well up until today.

    Generating Profile with the default values works. Changing some values in ways that create error conditions works. However, a previously working profile now crashes when Generate Profile is clicked.

    This profile was confirmed with TES. 

    I reinstalled the wizard. I reinstalled the matlab runtime. There's nothing in Windows Temp that looks related. 

    Windows 10, current with updates. 

    -Abraxas3d

Reply
  • Same problem here! I came here to try and find out what to do because I'm baffled. 

    Talise Configuration Wizard version 2.4 installed. 

    It has worked well up until today.

    Generating Profile with the default values works. Changing some values in ways that create error conditions works. However, a previously working profile now crashes when Generate Profile is clicked.

    This profile was confirmed with TES. 

    I reinstalled the wizard. I reinstalled the matlab runtime. There's nothing in Windows Temp that looks related. 

    Windows 10, current with updates. 

    -Abraxas3d

Children