Post Go back to editing

Frequency hopping GPIO mode tuning issue

Category: Software
Product Number: ADRV9009
Software Version: 3.6.2.1

HI Team,

I am working ZCU102 interface with ADRV9009,we are using Frequency hopping GPIO mode function ,when we are changing frequency from one to another we observe that we are not getting the LO that we have tuned. When we call the hopping function in a continuous loop we are able to see that the LO is being set. When we call it once or twice it is not working. Could you please guide to resolve this issue?

Parents
  • Please confirm whether you are using the ZCU102 board with the ADRV900x evaluation board. Are you using the GPIO mode to control the frequency change? If you are using the GPIO mode and need to assign frequency hopping GPIO during initialization time, the next hopping frequency must be set via an API command. Please refer to the RF PLL FREQUENCY HOPPING section in the ADRV900x reference manual.

Reply
  • Please confirm whether you are using the ZCU102 board with the ADRV900x evaluation board. Are you using the GPIO mode to control the frequency change? If you are using the GPIO mode and need to assign frequency hopping GPIO during initialization time, the next hopping frequency must be set via an API command. Please refer to the RF PLL FREQUENCY HOPPING section in the ADRV900x reference manual.

Children
No Data