Post Go back to editing

ADRV9009 transeciver evaluation software, Lane rate is 0

Category: Software
Product Number: ADRV9009
Software Version: 3.6.1.2

when i use ADRV9009 transceiver evaluation software , i set up the rx bandwidth, sample rate, tx bandwidth ..etc ; but the jesd 204b page , the lane rate always shows

such error,  the lane rate is 0;  the lane rate set two low. 

whatever i set the rx/tx parameter , the 204B lane rate is still 0.  how can i solve this problem ?

Parents Reply Children
  • Translation: 

    I have seen the evaluation software you sent, but mainly I want to ask if there is any configuration 
    software for adrv9009. Can the evaluation software configure the RF transceiver?

    我看过您发送的评估软件,但我主要想问一下是否有适用于adrv9009的配置软件。评估软件可以配置射频收发器吗?

  • Can you try with the attached profile and see if its working fine . 

    <GUI_Setup>
      <Device>ADRV9009</Device>
      <DeviceClock>245.76MHz</DeviceClock>
      <TxChannel>TX1 and TX2 Enabled</TxChannel>
      <TxProfile>Tx 100/225MHz, IQrate 245.76MHz</TxProfile>
      <ObsProfile>ORX 200MHz, IQrate 245.76MHz, Dec4</ObsProfile>
      <RxChannel>RX1 and RX2 Enabled</RxChannel>
      <RxProfile>Rx 100MHz, IQrate 122.88MHz, Dec4</RxProfile>
      <RxPllFreq>1800</RxPllFreq>
      <RxPllExtLo>NO</RxPllExtLo>
      <Tx1InitAttenuation>0</Tx1InitAttenuation>
      <Tx2InitAttenuation>0</Tx2InitAttenuation>
      <RxFramerSelection>Framer A</RxFramerSelection>
      <TxFramerSelection>Deframer A</TxFramerSelection>
      <ObsRxFramerSelection>Framer A</ObsRxFramerSelection>
      <UseExternalSysRef>True</UseExternalSysRef>
      <FramerALane0>True</FramerALane0>
      <FramerALane1>False</FramerALane1>
      <FramerALane2>False</FramerALane2>
      <FramerALane3>False</FramerALane3>
      <FramerAScrambling>True</FramerAScrambling>
      <FramerARelink>False</FramerARelink>
      <FramerAK>32</FramerAK>
      <FramerAKOffset>31</FramerAKOffset>
      <FramerBLane0>True</FramerBLane0>
      <FramerBLane1>False</FramerBLane1>
      <FramerBLane2>False</FramerBLane2>
      <FramerBLane3>False</FramerBLane3>
      <FramerBScrambling>True</FramerBScrambling>
      <FramerBRelink>False</FramerBRelink>
      <FramerBK>32</FramerBK>
      <FramerBKOffset>31</FramerBKOffset>
      <DeframerALane0>True</DeframerALane0>
      <DeframerALane1>True</DeframerALane1>
      <DeframerALane2>False</DeframerALane2>
      <DeframerALane3>False</DeframerALane3>
      <DeframerAScrambling>True</DeframerAScrambling>
      <DeframerARelink>False</DeframerARelink>
      <DeframerAK>32</DeframerAK>
      <DeframerAKOffset>17</DeframerAKOffset>
      <DeframerBLane0>False</DeframerBLane0>
      <DeframerBLane1>False</DeframerBLane1>
      <DeframerBLane2>True</DeframerBLane2>
      <DeframerBLane3>True</DeframerBLane3>
      <DeframerBScrambling>True</DeframerBScrambling>
      <DeframerBRelink>False</DeframerBRelink>
      <DeframerBK>32</DeframerBK>
      <DeframerBKOffset>17</DeframerBKOffset>
      <RxQECInit>True</RxQECInit>
      <TxQECInit>True</TxQECInit>
      <InternalTxLOLInit>True</InternalTxLOLInit>
      <ExternalTxLOLInit>False</ExternalTxLOLInit>
      <Rx1QECTrack>False</Rx1QECTrack>
      <Rx2QECTrack>False</Rx2QECTrack>
      <Rx1Hd2Track>False</Rx1Hd2Track>
      <Rx2Hd2Track>False</Rx2Hd2Track>
      <Tx1QECTrack>False</Tx1QECTrack>
      <Tx2QECTrack>False</Tx2QECTrack>
      <Tx1LOLTrack>False</Tx1LOLTrack>
      <Tx2LOLTrack>False</Tx2LOLTrack>
      <Orx1QECTrack>False</Orx1QECTrack>
      <Orx2QECTrack>False</Orx2QECTrack>
    </GUI_Setup>