Post Go back to editing

ADRV9009 transeciver evaluation software, Lane rate is 0

Category: Software
Product Number: ADRV9009
Software Version: 3.6.1.2

when i use ADRV9009 transceiver evaluation software , i set up the rx bandwidth, sample rate, tx bandwidth ..etc ; but the jesd 204b page , the lane rate always shows

such error,  the lane rate is 0;  the lane rate set two low. 

whatever i set the rx/tx parameter , the 204B lane rate is still 0.  how can i solve this problem ?

Parents Reply Children
  • Are you still facing the issue? If not, can you send us the profile that you are using?

    Go to TES GUI, then to File and save the GUI setup in xml format and then share that with us

  • Translation: 

    I have seen the evaluation software you sent, but mainly I want to ask if there is any configuration 
    software for adrv9009. Can the evaluation software configure the RF transceiver?

    我看过您发送的评估软件,但我主要想问一下是否有适用于adrv9009的配置软件。评估软件可以配置射频收发器吗?

  • Can you try with the attached profile and see if its working fine . 

    <GUI_Setup>
      <Device>ADRV9009</Device>
      <DeviceClock>245.76MHz</DeviceClock>
      <TxChannel>TX1 and TX2 Enabled</TxChannel>
      <TxProfile>Tx 100/225MHz, IQrate 245.76MHz</TxProfile>
      <ObsProfile>ORX 200MHz, IQrate 245.76MHz, Dec4</ObsProfile>
      <RxChannel>RX1 and RX2 Enabled</RxChannel>
      <RxProfile>Rx 100MHz, IQrate 122.88MHz, Dec4</RxProfile>
      <RxPllFreq>1800</RxPllFreq>
      <RxPllExtLo>NO</RxPllExtLo>
      <Tx1InitAttenuation>0</Tx1InitAttenuation>
      <Tx2InitAttenuation>0</Tx2InitAttenuation>
      <RxFramerSelection>Framer A</RxFramerSelection>
      <TxFramerSelection>Deframer A</TxFramerSelection>
      <ObsRxFramerSelection>Framer A</ObsRxFramerSelection>
      <UseExternalSysRef>True</UseExternalSysRef>
      <FramerALane0>True</FramerALane0>
      <FramerALane1>False</FramerALane1>
      <FramerALane2>False</FramerALane2>
      <FramerALane3>False</FramerALane3>
      <FramerAScrambling>True</FramerAScrambling>
      <FramerARelink>False</FramerARelink>
      <FramerAK>32</FramerAK>
      <FramerAKOffset>31</FramerAKOffset>
      <FramerBLane0>True</FramerBLane0>
      <FramerBLane1>False</FramerBLane1>
      <FramerBLane2>False</FramerBLane2>
      <FramerBLane3>False</FramerBLane3>
      <FramerBScrambling>True</FramerBScrambling>
      <FramerBRelink>False</FramerBRelink>
      <FramerBK>32</FramerBK>
      <FramerBKOffset>31</FramerBKOffset>
      <DeframerALane0>True</DeframerALane0>
      <DeframerALane1>True</DeframerALane1>
      <DeframerALane2>False</DeframerALane2>
      <DeframerALane3>False</DeframerALane3>
      <DeframerAScrambling>True</DeframerAScrambling>
      <DeframerARelink>False</DeframerARelink>
      <DeframerAK>32</DeframerAK>
      <DeframerAKOffset>17</DeframerAKOffset>
      <DeframerBLane0>False</DeframerBLane0>
      <DeframerBLane1>False</DeframerBLane1>
      <DeframerBLane2>True</DeframerBLane2>
      <DeframerBLane3>True</DeframerBLane3>
      <DeframerBScrambling>True</DeframerBScrambling>
      <DeframerBRelink>False</DeframerBRelink>
      <DeframerBK>32</DeframerBK>
      <DeframerBKOffset>17</DeframerBKOffset>
      <RxQECInit>True</RxQECInit>
      <TxQECInit>True</TxQECInit>
      <InternalTxLOLInit>True</InternalTxLOLInit>
      <ExternalTxLOLInit>False</ExternalTxLOLInit>
      <Rx1QECTrack>False</Rx1QECTrack>
      <Rx2QECTrack>False</Rx2QECTrack>
      <Rx1Hd2Track>False</Rx1Hd2Track>
      <Rx2Hd2Track>False</Rx2Hd2Track>
      <Tx1QECTrack>False</Tx1QECTrack>
      <Tx2QECTrack>False</Tx2QECTrack>
      <Tx1LOLTrack>False</Tx1LOLTrack>
      <Tx2LOLTrack>False</Tx2LOLTrack>
      <Orx1QECTrack>False</Orx1QECTrack>
      <Orx2QECTrack>False</Orx2QECTrack>
    </GUI_Setup>