Post Go back to editing

ADRV9009 Power level at 2.4GHz and 5.8GHz

Category: Choose a category

Hi everyone, 

i'm working with the ADRV9009-ZU11EG, i tried to generate a SinWave signal with a -35dBm power with a signal generator. I tried to measure this SinWave at 2.4GHz and 5.8GHz by means of power density spectrum computation. At 2.4GHz i found the signal magnitude which is correct regarding the generated signal. But at 5.8GHz i measure a signal level much lower than what expected (about 10dB lower). I would like to know why? and is there any solution to this issue?

Find bellow the measure power with the ADR9009 with 8 channels.

  2,4GHz (dBm) 5,8Ghz(dBm)
CH 0 -35 -45
CH 1 -35 -42,9
CH 2 -35 -40
CH 3 -35 -50
CH 4 -35 -45
CH 5 -35 -44
CH 6 -35 -45
CH 7 -35 -48

An example of time domain and frequency domaine signal mesured at 2.4GHz.

An example of time domain and frequency domaine signal mesured at 5.8GHz.

Kind regards

Ettien.K

Parents Reply Children
No Data