Hello,
I have the ZCU102 booting and running the 2018-R2-2019_05_23.img. When I manually set the board IP address I can ping the board from my PC. But the TES GUI cannot connect to the ZCU102 - ADRV9009. I saw in an old post (April 2019) that TES was not supported on ZCU102. Is TES now supported? If not, when will it be, and what are my other options? I need to configure the 9009 via TES and generate C files for my no_OS build.
Thanks,
Keith