The TES GUI can have resolution issues after a fresh install. This is a result of the PC system settings. Commonly the GUI will look like this with the tab on top of each other.

How to fix this issue:
- Navigate to the source of the .exe. Its is called Argo.Navis.exe and can be found in the default location at C:\Program Files\Analog Devices\ADRV9001 Transceiver Evaluation Software
- Right click on the .exe file and open the Properties menu.
- in the compatibility tab select the Change high DPI settings button
- In the High DPI scaling behaviour make sure this is set to System.
- Click OK and re-open the TES GUI.