I want to test evaluate the Hopping modes and timings on the ADRV9002 Transceiver.
I have been able to get the hopping to work using TDD (Time Division Duplexing), i now want to use an external trigger such as the rising edge of a wave from a waveform generator to trigger a hop to the next frequency.
I have tried using the GPIO pins currently D-GPIO 2 however the eval board seem to be outputting a signal, the oscilloscope shows high to low fluctuations (1 & 0) states.
- What are the differences between the Hop pin, GPIO Trigger and SPI Trigger?
- How can I trigger hopping with an external trigger such as a waveform generator?
Any Help is appreciated, Thank you






Above is the hop table, What's the difference between hop index and code?