Post Go back to editing

Can't get Rx1A_In to output in TES

Category: Hardware
Product Number: ADRV9002

i have been following the instructions as per  3) Transmit/Receive Example i have been able to get Tx to work but after conecting a SMC100A signal generator to RX1A_IN i was unable to pick up a signal.

What can i do to solve this? I Saw another post about using a feedback loop here  RE: ADRV9002 Loopback Rx to Tx 

Thank you,

Oliver

Thread Notes

Parents Reply
  • Hi Oliver,

    As you mentioned in the previous statement that the loopback from TX to Rx is working fine. This tells us that the Rx is programmed and working fine. After inspecting your taxidi file I can see that the carrier frequency that is provided is 900 MHz and the data port sample rate is 48kSPS. 

    Since your transmitter is transmitting the signal at 900MHz, that's the reason why the Tx-RX loop is working. 

    Please set the same carrier frequency around 900MHz +/- 24kHz in the signal generator. The range of signal that the Rx is going to capture is determined by the dataport sample rate i.e., 48kSPS/2 (+/-24kHz). 

    I hope this will resolve the issue. 

    Regards

    Rahul 

Children