Post Go back to editing

Can't get Rx1A_In to output in TES

Category: Hardware
Product Number: ADRV9002

i have been following the instructions as per  3) Transmit/Receive Example i have been able to get Tx to work but after conecting a SMC100A signal generator to RX1A_IN i was unable to pick up a signal.

What can i do to solve this? I Saw another post about using a feedback loop here  RE: ADRV9002 Loopback Rx to Tx 

Thank you,

Oliver

Thread Notes

Parents
  • Often there's confusion between Rx1A and Rx1B ports. Please ensure that your intended Rx RF input port is the one connected to your signal generator. Also make sure that your signal's RF center frequency falls within the band of your receiver (carrier frequency +/- RF bandwidth). If you start a default TES v26 session, just choose FDD as duplex mode, add wired loopback with proper attenuation between Tx1 and Rx2, you should receive a single tone generated in transmit tab.

    Best,

    Stefan

  • Hi, 

    i was able to get Rx working using a feedback loop to Tx. i was able to see Rx plot on TES GUI. when using s signal generator i was unable to see a signal on the recieve page. 

  • Hi Oliver,

    What kind of signal are you trying to send? I'm assuming it's a single tone you're feeding into Rx1A, what's your signal generator's tone frequency and power? Based on the profile you provided you should see a signal within a range of 900MHz +/- 6kHz.

    Best,

    -Stefan

Reply Children