Post Go back to editing

Can't get Rx1A_In to output in TES

Category: Hardware
Product Number: ADRV9002

i have been following the instructions as per  3) Transmit/Receive Example i have been able to get Tx to work but after conecting a SMC100A signal generator to RX1A_IN i was unable to pick up a signal.

What can i do to solve this? I Saw another post about using a feedback loop here  RE: ADRV9002 Loopback Rx to Tx 

Thank you,

Oliver

Thread Notes

Parents
  • Often there's confusion between Rx1A and Rx1B ports. Please ensure that your intended Rx RF input port is the one connected to your signal generator. Also make sure that your signal's RF center frequency falls within the band of your receiver (carrier frequency +/- RF bandwidth). If you start a default TES v26 session, just choose FDD as duplex mode, add wired loopback with proper attenuation between Tx1 and Rx2, you should receive a single tone generated in transmit tab.

    Best,

    Stefan

Reply
  • Often there's confusion between Rx1A and Rx1B ports. Please ensure that your intended Rx RF input port is the one connected to your signal generator. Also make sure that your signal's RF center frequency falls within the band of your receiver (carrier frequency +/- RF bandwidth). If you start a default TES v26 session, just choose FDD as duplex mode, add wired loopback with proper attenuation between Tx1 and Rx2, you should receive a single tone generated in transmit tab.

    Best,

    Stefan

Children