Hello,
I am trying to connect to TES. My hardware is an EVAL-ADRV9002 and a ZCU102 dev board.
I can see there are 2 softwares for the FPGA
1. I currently have the navassa_ZCU102 img file from this link https://www.analog.com/en/lp/001/transceiver-evaluation-software.html on an SD card.
2. Engineer zone has linked me to a Kuiper image file.
Which one do i need in order to connect with TES?
The quickstart manual mentions using ip adress 192.168.1.2. However the boards ip is set to 192.168.1.10. As far as i am aware i use an ethernet connection and set a static ip to 192.168.1.10 which i use in TES. Is this correct?
Any Help is appreciated