Post Go back to editing

Running multiple channels in independent mode while using ZCU102 with ADRV9002.

Category: Software
Product Number: ADRV9002

I tried the ADRV902_DDS_Example from Analog Devices Transceiver toolbox and it worked fine. I could visualize the output sine waveforms.

But when I change the EnabledChannels property to [1,2], I am getting the below error:

Does this mean we can only use one channel either 1 or 2 in Independent mode? Am I missing something?



Updated subject to reflect the question
[edited by: Alekhya2609 at 6:25 PM (GMT -5) on 8 Feb 2024]

Thread Notes