Hello,
I am unable to connect using TES to ADRV9002 and ZC706 Combo.
My setup is ADRV9002NP/W1/PCBZ + ZC706 (Avnet logo board).
The PC is set to 192.168.1.2 and connected to ZC706. However, I am not able to connect using TES to 192.168.1.10 (ZC706).
Furthermore, I am not able to ping 192.168.1.10 address, so I guess the issue is not the TES software but the Board or SD cards.
I have tried both the SD card that was shipped with the ADRV9002 board labelled "for ADRV9001 TES software R0.2 2020.12" and the SD card that I have created using the instructions on the AD website:
Using any card I am not able to ping 192.168.1.10.
The LED are behaving as follows when using SD card created by using the instructions from the link:
On Z706 - PL GPIO LED - flashing in rolling manner with 3 on and 1 off left to right.
On ADRV9002 - DS501 ON, D801 - ON, DS703 System OK - flashing.
The PC is able to ping itself 192.168.1.2 when the ZC706 is powered on, but pings to 192.168.1.10 timeout.
Please advise how to troubleshoot the connectivity problem further.
[edited by: DSPdesigner at 9:09 AM (GMT -4) on 20 Apr 2022]