Post Go back to editing

Make a new SD card for the ADRV9002 SDK

My SD card got corrupted.

Where do I go to make a new SD card that will work for the ZC706 and the ADRV9002?

I want to make sure I duplicate the same SD card that came with the board.

Thanks

Charly



fixed the fpga board name
[edited by: charlyelkhoury at 1:13 PM (GMT -4) on 19 Aug 2020]
Parents Reply
  • Hi,

    I downloaded the "adrv9001_legacy_sdcard.zip" and manually kept in Local/Temp directory as mentioned and clicked format sd card.

    It opened the disk imager and gave the path Local/Temp/**sdcard**.zip . and then, device point to sdcard.

    The problem is when i click write to device, it throughs error as "Unable to init write to device. End of Central Directory record could not be found".

    Can u explain what is this error and why i am unable to write to device.

Children