Post Go back to editing

ADRV9371-W/PCBZ+EVAL-TPG-ZYNQ3 setup

Category: Software
Product Number: AD9371

Hi team,

I used ethernet cable to connect EVAL-ZYNQ3 board with PC. And connect ZYNQ3 board with ADRV9371- W/PCBZ board.

Then give the 12V power supply. The indicator LED on these two boards are both lighted.

But AD9371 GUI indicated that zynq platform is disconnected.

How to solve this problem? Do I need to install some driver on PC?

When I change AD9371 to AD9361-EVAL-BOARD, there is the same phenomenon "device not detected".

Could you help answer this question? 

Thanks!