Post Go back to editing

ad9371 ORX noise raised at frequency edges

Category: Hardware
Product Number: ad9371

Settings:

ad9371 orx IQrate 245.76MHz, bandwidth 200MHz, 

Using the following Orx filter config generated by ad9371 filter wizard 

<obs>
<adcDiv=1>
<rxFirDecimation=1>
<rxDec5Decimation=5>
<enHighRejDec5=1>
<rhb1Decimation=1>
<iqRate_kHz=245760>
<rfBandwidth_Hz=200000000>
<rxBbf3dBCorner_kHz=100000>

<filter FIR gain=6 num=24>
-289
81
-23
-86
229
-354
397
-233
-657
1699
-4172
23010
-4172
1699
-657
-233
397
-354
229
-86
-23
81
-289
0
</filter>

But the received orx signal has raised noise at frequency edge.

if i turn off the signal, the noise looks not flat,check the red curve in following figure.

I try some dec5 filter coefs, no big change. 

thanks 

Parents
  • I have seen noise peaking like this before and it was due to noise aliasing.  If the BW of the decimating filter is slightly too wide, you tend to the see the higher frequency noise increase.  Hope this helps.

    This is a random response to the last post.  I haven't read the other posts.

Reply
  • I have seen noise peaking like this before and it was due to noise aliasing.  If the BW of the decimating filter is slightly too wide, you tend to the see the higher frequency noise increase.  Hope this helps.

    This is a random response to the last post.  I haven't read the other posts.

Children