Post Go back to editing

AD9375 Sampling rate issue

Category: Software
Software Version: 2019R2

Hello,

I am using ADRV9375 with ZC706 and using 2019R2 version of HDL and No-OS application.

I want to change My Tx IQ rate to 122.88MSPS, in No-OS application default it is set to 245.76MSPS when I configured Tx IQ rate to 122.88MSPS JESD lane is getting stuck at ILAS state, error log is added below

/cfs-file/__key/communityserver-discussions-components-files/439/log_5F00_tx_5F00_122p88msps_5F00_iq_5F00_rate.txt

log_tx_245p76msps_iq_rate log file contains log with TX IQ rate set to 245.76MSPS(default) -- Log is proper and JESD is in DATA state.
log_tx_122p88msps_iq_rate log file contains log with TX IQ rate set to 245.76MSPS-- JESD is in ILAS state.
TX profile for 245.76MSPS IQ rate :

static mykonosTxProfile_t txProfile =
/* Tx 75/200MHz, IQrate 245.76MSPS, Dec5 */
    DACDIV_2p5,     /* The divider used to generate the DAC clock*/
    &txFir,         /* Pointer to Tx FIR filter structure*/
    1,              /* The Tx digital FIR filter interpolation (1,2,4)*/
    2,              /* Tx Halfband1 filter interpolation (1,2)*/
    1,              /* Tx Halfband2 filter interpolation (1,2)*/
    1,              /* TxInputHbInterpolation (1,2)*/
    245760,         /* Tx IQ data rate in kHz*/
    75000000,       /* Primary Signal BW*/
    200000000,      /* The Tx RF passband bandwidth for the profile*/
    189477,         /* The DAC filter 3dB corner in kHz*/
    100000,         /* Tx BBF 3dB corner in kHz*/
    0               /* Enable DPD, only valid for AD9373*/
};
 
TX profile for 122.88MSPS IQ rate :
 
//Tx IQrate 122.88MSPS
static mykonosTxProfile_t txProfile =
/* Tx 20/100MHz, IQrate 122.88MSPS, Dec5 */
DACDIV_2p5,     /* The divider used to generate the DAC clock*/
&txFir,         /* Pointer to Tx FIR filter structure*/
2,              /* The Tx digital FIR filter interpolation (1,2,4)*/
2,              /* Tx Halfband1 filter interpolation (1,2)*/
1,              /* Tx Halfband2 filter interpolation (1,2)*/
1,              /* TxInputHbInterpolation (1,2)*/
122880,         /* Tx IQ data rate in kHz*/
20000000,       /* Primary Signal BW*/
100000000,      /* The Tx RF passband bandwidth for the profile*/
710539,         /* The DAC filter 3dB corner in kHz*/
50000,          /* Tx BBF 3dB corner in kHz*/
0               /* Enable DPD, only valid for AD9373*/
};
Please suggest me how to proceed further.
Regards,
Jaydeep
 
Parents Reply Children
No Data